You are here: KAS IDE Reference > Project Structure

Create Programs

This chapter provides details on the syntax, structure and use of the declarations and statements supported by the KAS IDE"Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger application language.

Project Structure

Structuring the application with care is important in creating your project (see Project Structure Guidelines in Advanced Topics).

IEC 61131-3 Editors

The KAS IDE programming environment provides language dedicated editors for:

A more extensive description on each language can be found in the following sections of the Technical References:

See also Program Limitations and the PLC Online Change feature.

Some Tips...

About Drag-and-Drop

The editor provides you with an ideal programming environment, including drag-and-drop features:

About Autocompletion

When you type the name of a function block instance (use either as an instance or a data structure), pressing the point "." after the name of the instance opens a pop-up list with the names of possible elements. Click the relevant element and validate it with the check mark.

Autocompletion

Figure 4-79: Autocompletion

Auto-completion of words

About tooltip on variable

When you leave the mouse cursor on a variable in Editors, a tooltip is displayed to give you more details on the item.

Tooltip on Variable

Figure 4-80: Tooltip on Variable

The header of the tooltip displays the name of the variable and its type.

About Bookmarks 

See Bookmarks

Select Function Blocks

All available Operators, functions and function blocks are listed in the Libraries toolbox. The list of available blocks is sorted into categories. The “(All)” category enables you to see the complete list of available blocks.

To insert a block in a program, select it and drag-and-drop it to the desired position in the Editor.

Select Variables and Instances

Symbols of variables and instances are selected using the variable list in the Dictionary. Selecting variables is available from all editors:

Concept Link IconSee Also

 

Project Structure

IEC 61131 Editors

Drag and Drop Programming

Autocompletion When Programming

Tooltips on Variables

Selecting Function Blocks

Selecting Variables and Instances

Change Functions and Operators in FFLD and FBD Editors

Change Function Blocks in FFLD and FBD Editors

SFC Editor

FBD Editor

ST / IL Editor

FFLD Editor


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™